AXIS#.MOTOR.TEMPWARN
Description
This parameter is used to configure the motor temperature warning level as a resistance threshold of the motor PTC.
A zero value prevents any warning from being created.
Context
For more information see Motor and Motor Temperature View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Ω |
|
Range |
0 to 2,000,000,000 Ω |
|
Default Value |
0 Ω = switched off |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.TEMPWARN |
500bh |
1eh |
Unsigned32 |
- |
- |
Read/Write |
No |
|
AXIS2.MOTOR.TEMPWARN |
510bh |
1eh |
Unsigned32 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6219 |
1 |
6219 (0x184b) |
AXIS1.MOTOR.TEMPWARN |
Unsigned32 |
Read/Write |
Yes |
|
71755 |
2 |
6219 (0x184b) |
AXIS2.MOTOR.TEMPWARN |
Unsigned32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.TEMPWARN |
6219 |
Unsigned32 |
Read/Write |
- |