VBUS.INRUSHON

Description

This parameter returns the voltage at which the DC bus inrush relay closes.

Examples

Usage

The drive configures this parameter based on power electronics component ratings. When the measured DC bus voltage VBUS.VALUE is greater than VBUS.INRUSHON, the drive closes the inrush relay.

Context

For more information on DC bus operation, refer to Power.

Versions

Action Version Notes
Implemented 02-02-03-000  

General Information

Type

Read Only

Units

VDC

Range

N/A

Default Value

N/A

Data Type

Integer

See Also VBUS.VALUE, VBUS.INRUSHOFF

Stored in Non-Volatile Memory

No

Variants Supported

All variants supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2506

1

2506 (0x9ca)

VBUS.INRUSHON

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.INRUSHON

2506

Unsigned16

Read Only

-