Power View

From the Power screen, you can view and configure the drive power settings as follows.

Section Element Description Parameter Parameter
Voltage VBus Gauge A graphical gauge representation of the DC bus voltage, including ranges for warnings and faults. The slider adjusts the zoom level of the gauge. VBUS.VALUE VBUS.VALUE
Under Voltage Fault Threshold Sets the value at which an under voltage fault will occur

VBUS.UVFTHRESH

VBUS.UVFTHRESH
Under Voltage Warning Threshold Sets the value at which an under voltage warning will occur VBUS.UVWTHRESH VBUS.UVWTHRESH
Actual Value Displays the current actual voltage value VBUS.VALUE VBUS.VALUE
Over Voltage Warning Threshold Sets value at which an over voltage warning will occur. Setting a value of 0 generates no warning. VBUS.OVWTHRESH VBUS.OVWTHRESH
Over Voltage Fault Threshold Sets value at which an over voltage fault will occur VBUS.OVFTHRESH VBUS.OVFTHRESH
Under Voltage Fault Mode Sets the behavior for when an under voltage fault are monitored. VBUS.UVMODE VBUS.UVMODE
Input Input Mains Sets whether the mains input is DC or AC. VBUS.DCOPERATION
Nominal AC Line Sets the operating voltage of the drive. VBUS.ACNOMINAL  
AC Line Phases Sets whether the AC line input to the DC bus is single or three phase, and whether phase loss detection is active. VBUS.THREEPHASE  
Input Input Mains Sets whether the mains input is DC or AC.   VBUS.DCOPERATION
Operating Voltage Used to change voltage thresholds, allowing -07 drive types to work at a -06 drive's voltage threshold.   VBUS.HALFVOLT
DC-Bus Share Precharge Timeout Sets a timeout for the MKD-C's precharge process.   VBUS.PRECHARGETO
Output Voltage - Disable Mode (All Strings Tab) Used to keep drives connected to MKD-C enabled, even when the MKD-C loses its high voltage supply.   STRINGS.DISMODE
Actual Output Voltage (String 1-3 Tabs) Displays the actual output voltage on the individual string.   STRINGx.VVALUE
Total Current - Actual Value (All Strings Tab) Displays the combined current of all strings.   STRINGS.IVALUE
Current - Actual Value (String 1-3 Tabs) Displays the current of the individual string.   STRINGx.IVALUE
Current Warning Threshold (All Strings Tab) Sets the combined warning threshold of the individual strings.   STRINGS.IWTHRESH
Current Warning Threshold (String 1-3 Tabs) Sets the warning threshold for the individual string.   STRINGx.IWTHRESH
Current Fault Threshold (All Strings Tab) Displays the combined fault threshold of all strings.   STRINGS.IFTHRESH
Current Fault Threshold (String 1-3 Tabs) Displays the fault threshold of the individual string.   STRINGx.IFTHRESH
Total Power - Actual Value (All Strings Tab) Displays the combined total percentage of output power of all strings   STRINGS.I2TVALUE
Power - Actual Value (String 1-3 Tabs)

Displays the total percentage of output power for the individual string.

  STRINGx.I2TVALUE
Power Warning Threshold (All Strings Tab) Sets the combined output power warning threshold percentage of all the strings.   STRINGS.I2TWTHRESH
Power Warning Threshold (String 1-3 Tabs) Sets the output power warning threshold percentage of the individual string.   STRINGx.I2TWTHRESH
Power Fault Threshold (All Strings Tab) Displays the combined output power fault threshold percentage of all the strings.   STRINGS.I2TFTHRESH
Power Fault Threshold (String 1-3 Tabs) Displays the combined output power fault threshold percentage of the individual string.   STRINGx.I2TFTHRESH

See Regeneration for more information about regen resistors and sizing regen resistors. 

Operating Voltage

Operating voltage can be selected by the user to allow 480VAC drives to work on 240VAC input supplies.

The VBUS.ACNOMINAL parameter has an effect on the following voltage-thresholds:

  1. DC-bus over-voltage threshold (see VBUS.OVFTHRESH).
  2. The regen-resistor enable/disable voltage thresholds.
  3. The inrush-relay enable/disable voltage thresholds.

A power-cycle is needed after changing the value and saving the parameter on the NV memory of the Drive, since the voltage thresholds mentioned above are read during the boot-sequence of the drive.