AXIS#.HWEN.MODE

Description

Selects whether AXIS#.CLRFAULTS is performed on the rising edge of the hardware enable input

Examples

Usage

0 (default): perform AXIS#.CLRFAULTS on the rising edge of the hardware enable input

1: do not perform clear faults on the rising edge of the hardware enable input

Code

--> AXIS1.HWEN.MODE 0
--> AXIS2.HWEN.MODE 1

Context

For more information on hardware enable, refer to Enable/Disable.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.HWEN.SOURCE, AXIS#.HWEN.STATE, AXIS#.CLRFAULTS

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HWEN.MODE

5009h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7000

1

7000 (0x1b58)

AXIS1.HWEN.MODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HWEN.MODE

7000

Unsigned8

Read/Write

-