Motion Library
- The KAS function library contains ML function blocks used to integrate motion in a PLC program.
- ML function blocks can be used in four of the IEC 61131-3 languages: ST, FBD, FFLD and IL.
- For Sequential Function Chart (SFC) programs, ML function blocks are used as part of SFC Steps or SFC Transitions defined with FBD, FFLD, IL, or ST languages.