Sequential Function Chart (SFC)
- Graphical steps are used to represent stable states.
- Transitions describe the conditions and events that lead to a change of state.
- Using SFC simplifies the programming of sequential operations because it saves a lot of variables and tests just for maintaining the program context.
-
-
Do not use SFC as a decision diagram.
Using a step as a point of decision and transitions as conditions in an algorithm must never appear in an SFC chart.
Using SFC as a decision language leads to poor performance and complicate charts.
ST is preferred when programming a decision algorithm that has no sense in terms of program state.
These are basic components of an SFC chart:
|
Chart |
Programming |
|---|---|
The KAS-IDE fully supports SFC programming with several hierarchical levels of charts (e.g., a chart that controls another chart).
Working with a hierarchy of SFC charts is an easy and powerful way for managing complex sequences and saves performances at runtime.
See:
See Also