PL.ERR

Description

PL.ERR reads the position error present when the drive is controlling the position loop. PL.ERR is the difference between the actual position of the motor shaft (PL.FB) and the commanded position of the drive (PL.CMD).  If the drive is not in the position operating mode (DRV.OPMODE = 2), then the PL.ERR value is not generated by the drive and this parameter is read as 0.

AKD BASIC Notes


  • When you enable the position error interrupt (by setting INTR.PL.ERR=1), the Position Error fault is disabled. In situations where it would have occurred, a position error interrupt is generated instead.

General Information

Type

R/O Parameter

Units

counts, rad, deg, (custom units)

Range

N/A  

Default Value

N/A

Data Type

Float

BASIC: Integer

See Also

PL.FB

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

35C5h/0

60F4h/0

M_01-00-00-000

Related Topics

PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop