Baud_Rate
Baud_Rate
| Address: | 16569 (40B9H) |
| Type: | WORD |
| Access: |
Read or Read/Write |
| Unit: | mV |
| Range: | 0 to 7 (Modbus: 0 = 115.2k, 1= 57.6k, 2 = 38.4k, 3 = 19.2k, 4 = 9.6k, 5 = 4.8k, 6 = 2.4k, 7 = 1.2) |
| Default Value: |
-- |
| Store Supported: |
Yes |
| Description: |
This object contains the drive's Node Id. On drives with dip-switches/rotoswitches the object is read-only. On drives without dip-switches/rotoswitches this object can be changed using the KOLLMORGEN Space or following the procedure explained at §10.1.2. |
| Notes: |
-- |