Direct_Command_CMD

Direct_Command_CMD

Address:  16645 (4105H)
Type: UINT8
Access: Read/Write
Unit: --
Range: 0 (Stop motor movement) to 1 (Start motor movement)

Default Value:

--

Store Supported: No
Description:

This object enable the master to start or stop the drive’s motor. According to the desired command (move or stop) the Parameters #1, #2 assume the following meaning:

STOP Command (Direct_Command_CMD = 0)

Par #1 Value Par #1 Description Par #2 Value Par #2 Description

0

Stop with no ramp

Not used

Not used

1

Stop with ramp

Not used

Not used

2

Stop with steps

# Steps

Number of stop steps

20

SYNC Stop with no ramp

Not used

Not used

21

SYNC Stop with ramp

Not used

Not used

22

SYNC Stop with steps

# Steps

Number of stop steps

30

TRIGGER Stop with no ramp

Not used

Not used

31

TRIGGER Stop with ramp

Not used

Not used

32

TRIGGER Stop with steps

# Steps

Number of stop steps

 

 MOVE Command (Direct_Command_CMD = 1)

Par #1 Value

Par #1 Description

Par #2 Value

Par #2 Description

0

Move free running forward

Not used

Not used

1

Move free running backward

Not used

Not used

2

Move steps forward

# Steps

Number of movement steps

3

Move steps backward

# Steps

Number of movement steps

4

Move to Target position

Position

Position to reach

5

Move absolute steps

# Steps

Number of absolute steps (if steps < 0 move backward, if steps > 0 move forward)

10

Reserved

Not used

Not used

11

Reserved

Not used

Not used

16

Reserved

Not used

Not used

17

Reserved

Not used

Not used

20

Move free running forward with SYNC start

Not used

Not used

21

Move free running backward with SYNC start

Not used

Not used

22

Move steps forward with SYNC start

# Steps

Number of movement steps

23

Move steps backward with SYNC start

# Steps

Number of movement steps

24

Move to Target position with SYNC start

Position

Position to reach

25

Move absolute steps with SYNC start

# Steps

Number of absolute steps (if steps < 0 move backward, if steps > 0 move forward)

30

Move free running forward with TRIGGER start

Not used

Not used

31

Move free running backward with TRIGGER start

Not used

Not used

32

Move steps forward

with TRIGGER start

# Steps

Number of movement steps

33

Move steps backward

with TRIGGER start

# Steps

Number of movement steps

34

Move to Target position

with TRIGGER start

Position

Position to reach

35

Move absolute steps

with TRIGGER start

# Steps

Number of absolute steps (if steps < 0 move backward, if steps > 0 move forward)

Notes:

The Parameters objects Direct_Command_CMD must be configured first to write this object. If a parameter # is not used for the desired command it is not necessary to configure it. For more details about motor movement refers toTypes of Motor Movement.