Drive_Inputs_Setting
Drive_Inputs_Setting
| Address: | 8708 (2204H) | ||||||||||||||||||||||||||||||||||||
| Type: | DWORD | ||||||||||||||||||||||||||||||||||||
| Access: | Read/Write | ||||||||||||||||||||||||||||||||||||
| Unit: | -- | ||||||||||||||||||||||||||||||||||||
| Range: | 0 to 4294967295 | ||||||||||||||||||||||||||||||||||||
| Default Value: | 66064 | ||||||||||||||||||||||||||||||||||||
| Store Supported: | Yes | ||||||||||||||||||||||||||||||||||||
| Description: |
This register is used to parametrize drive digital inputs bank #0 allocation. For any function can be assigned one digital input that have to be specified in the four bits of register concerning that function.
|
||||||||||||||||||||||||||||||||||||
| Notes: | See Appendix. |