Feedback_Actual_Position_Error
Feedback_Actual_Position_Error
| Address: | 10266 (281AH) |
| Type: | INT32 |
| Access: | Read Only |
| Unit: | IU (one motor turn = 65536 IU) |
| Range: | INT32 |
| Default Value: | -- |
| Store Supported: | No |
| Description: |
This object returns the actual position displacement between MOTOR_REF_Position and the MOTOR_ACTUAL_Position. The value is refreshed if the feedback is active and the units are IU.
|
| Notes: | See Closed Loop Modality for details. |