Feedback_Calibration_Speed

Feedback_Calibration_Speed

Address: 10278 (2826H)
Type: UINT16
Access: Read/Write
Unit: 0.01 rpm
Range: 0 to 10000
Default Value: 500 (5 rpm)
Store Supported: Yes
Description: This value is used for Feedback feature and define motor speed during the calibration procedure. The value must be set at low speed. Generally 5 rpm is a good choice.
Notes: See Closed Loop Modality for details.