Feedback_Iq_Min

Feedback_Iq_Min

Address: 10259 (2813H)
Type: UINT16
Access: Read/Write
Unit: mA
Range: UINT16
Default Value:  500
Store Supported: Yes
Description: This value is used for Feedback feature and define the minimum amplitude of the phase’s current. Can be considered also as minimum current applied at the motor
Notes:

See Closed Loop Modality for details.