Feedback_Limit_Speed
Feedback_Limit_Speed
| Address:Address: | 10280 (2828H) |
| Type: | Unsigned32 |
| Access: | Read/Write |
| Unit: | rpm |
| Range: | Unsigned32 |
| Default Value: | 10000 |
| Store Supported: | Yes |
| Description: | This value is used for Feedback feature and define the maximum motor speed. If the speed became higher of the limit, the motor current is reduced to limit the speed. |
| Notes: | See Closed Loop Modality for details. |