Feedback_Settings

Feedback_Settings

Address: 10272 (2820H)
Type: UINT16
Access: Read/Write
Unit: rpm
Range:

UINT16

Default Value: 0
Store Supported: Yes
Description:

This value is used for Feedback feature and define some important settings about the feedback functionality. This object is managed at bit and the following tables show the meaning of each bits.

Feedback_Settings

15

14

13

12

11

10

9

8

7

6

5

4

3

2

1

0

 

 

 

 

Sensor Type

Calibration Mode

Kff_Switch

 

 

Type

0 ..3

 

Type: Mode

Mode 0: Compatibility Mode

Mode 1: Stop motor if position error reaches the limit and show drive Alarm

Mode 2: Stop motor if position error reaches the limit

Mode 3: Stop motor if velocity error reaches the limit and show drive Alarm

Mode 4: Stop motor if velocity error reaches the limit

Mode 5 to 15: Reserved

4

Not used

 

5

Not used

 

6

Kff_Switch

Define the managing of the feedforward current. See theGAIN tuning

7

Calibration Mode

0= the Strong Calibration is executed each time the Close Loop has to be activated  for example after the power is supplied or after an Reset Alarm that disabled the close loop

1= the Strong Calibration, is executed only the first time the power is supplied or when happen an Alarm that require the Strong Calibration (example encoder misalignment), in all other cases after the Reset_Alarm is sent, the Little Calibration will be done. See theGAIN tuning

8..11

 

Sensor Type

0 = incremental encoder

1 = Hall sensor

2 = incremental encoder + Hall sensor

3 = magnetic encoder

4 = absolute encoder multi turn SSI

5 = absolute encoder multi turn SSI + incremental encoder

6 = absolute encoder multi turn BISS

7 = absolute encoder multi turn BISS + incremental encoder

8 to 15 Reserved

12

Not used

 

13

Not used

 

14

Not used

 

15

Not used

 

Notes: See Closed Loop Modality for details.