Feedback_Source_PPR

Feedback_Source_PPR

Address: 10250 (280AH)
Type: Unsigned32
Access: Read/Write
Unit: Inc
Range: Unsigned32
Default Value: 1600
Store Supported: Yes
Description: This value is used for Feedback feature and define the quadrature pulses per revolution of incremental encoder installed on motor rear shaft.
Notes: See Closed Loop Modality for details.