Max_Current

Max_Current

Address: 4113 (1011H)
Type: WORD
Access: Read/Write
Unit: mA
Range: 0 to Max drive current
Default Value: 0
Store Supported: Yes
Description:

This should be set equal to the nominal current (A/Phase) of the motor per catalog specifications. It represents the motor’s current when running at constant speed.

Notes: The current set is the Irms current. The peak current is Irms * 1.4.