Min_Current
Min_Current
| Address: | 4112 (1010H) |
| Type: | WORD |
| Access: | Read/Write |
| Unit: | mA |
| Range: | 0 to Max drive current |
| Default Value: | 0 |
| Store Supported: | Yes |
| Description: |
It sets the motor’s reduced current. The drive automatically reduces the current after a current reduction time (Time_RWC object) at the end of the movement |
| Notes: | The current set is the Irms current. The peak current is Irms * 1.4. |