Motor_L

Motor_L

Address:  8194 (2002H)
Type: DWORD
Access: Read/Write
Unit: µH
Range: DWORD
Default Value: 2420
Store Supported: Yes
Description: This object sets the motor L (inductance). This value is used when bit #9 of Drive_Working_Settings_Extended object is equal to 0.
Notes:

--