Motor_SYNC

Motor_SYNC

Address: 8832 (2280H)
Type: WORD
Access: Write Only
Unit: --
Range: 0 to 1
Default Value: 0
Store Supported: No
Description: This object is used to synchronize the start and the stop of movement that must be synchronized between more axes.
Notes: See Movements with SYNC for details about synchronized movements.