Motor_Stall_Actual_Err_Angle
Motor_Stall_Actual_Err_Angle
| Address: | 8201 (2009H) |
| Type: | WORD |
| Access: | Read Only |
| Unit: | 0.01 radian |
| Range: | -32768 to 32767 |
| Default Value: | -- |
| Store Supported: | No |
| Description: |
This object returns the actual displacement between theoretical angle and estimated angle of motor rotor position for ‘Motor Stall detection’ feature. |
| Notes: | See Motor Stall Detection for more details about ‘Motor Stall detection' feature. This object is available only with firmware version V02r74 or superior. |