Motor_Stop_Trigger_Count
Motor_Stop_Trigger_Count
| Address: | 8784 (2250H) |
| Type: | WORD |
| Access: | Read/Write |
| Unit: | Edges |
| Range: | 0 to 65535 |
| Default Value: | 0 |
| Store Supported: | No |
| Description: | It defines the number of stop edges if a STOP with trigger input has been issued. Value = 0 means STOP at the first edge detected, Value = 1 means STOP after two edges detected, and so on. |
| Notes: | -- |