Node_Id
Node_Id
| Address: | 16568 (40B8H) |
| Type: | WORD |
| Access: | Read or Read/Write |
| Unit: | -- |
| Range: | 1 to 127 |
| Default Value: | 1 |
| Store Supported: | Yes |
| Description: | This object contains the drive's NodeId. On drives with dip-switches/rotoswitches the object is read-only. On drives without dip-switches/rotoswitches this object can be changed using the Kollmorgen Space or following the procedure explained at Baud Rate & Node Id Selection for Drives. |
| Notes: | -- |