Nominal_Current

Nominal_Current

Address: 4115 (1013H)
Type: WORD
Access: Read/Write
Unit: mA
Range: 0 to Max drive current
Default Value: 0
Store Supported: Yes
Description: It’s the motor’s nominal current (A/Phase) from the catalog specification. This parameter is used for the automatic detection of motor R/L. This parameter is generally set one time at initial setup when the motor is standstill. Each time the parameter is set to a different value, a new detection of R/L parameter is executed.
Notes: The current set is the Irms current. The peak current is Irms * 1.4.