Profile_Velocity
Profile_Velocity
| Address: | 4119 (1017H) |
| Type: | DWORD |
| Access: | Read/Write |
| Unit: | Hertz |
| Range: | 0 to Max_Profile_Velocity object included |
| Default Value: | 20000 |
| Store Supported: | Yes |
| Description: | It sets the motor velocity. |
| Notes: |
This object can also be set while the motor is running. This object must be lower than or equal to the Max_Profile_Velocity object. |