Stop_Trigger_Input_Filter

Stop_Trigger_Input_Filter

Address: 4434 (1152H)
Type: DWORD
Access: Read/Write
Unit: µs
Range: 0 to 4294967295
Default Value: 5242960
Store Supported: Yes
Description:

This object is used to set the filter for ‘Stop Trigger Input’.

Stop_Trigger_Input_Filter

 

(Digital Input High Level)

(Digital Input Low Level)

 

Bit 31 to 16

Bit 15 to 0

Range

0 to 65535

0 to 65535

Default Value

50h

50h

Notes:

--