Drive_Inputs_Setting
| Index.Sub | 2200.3H | ||||||||||||||||||||||||||||||||||||
| Data Type | Unsigned32 | ||||||||||||||||||||||||||||||||||||
| Access | Read/Write | ||||||||||||||||||||||||||||||||||||
| PDO Mappable | No | ||||||||||||||||||||||||||||||||||||
| Unit | -- | ||||||||||||||||||||||||||||||||||||
|
Range |
0 ÷ FFFFFFFFH | ||||||||||||||||||||||||||||||||||||
| Default Value | -- | ||||||||||||||||||||||||||||||||||||
| Store Supported | Yes | ||||||||||||||||||||||||||||||||||||
| Description |
This object is used to define drive digital inputs Bank #0 allocation used for functionality defined with bit#0, bit#1 and bit#2 of Drive_Working_Settings object. For any function can be assigned one digital input that have to be specified in the four bits of the object concerning that function.
0 = B0_IN0 digital input 4 = B0_IN4 digital input 1 = B0_IN1 digital input 5 = B0_IN5 digital input 2 = B0_IN2 digital input 6 = B0_IN6 digital input 3 = B0_IN3 digital input 7 = B0_IN7 digital input |
||||||||||||||||||||||||||||||||||||
|
Notes |