Max_Profile_Velocity
| Index.Sub | 607F.0H | ||||||
| Data Type | Unsigned32 | ||||||
| Access | Read/Write | ||||||
| PDO Mappable | RX_PDO (1) | ||||||
| Unit | User-defined velocity unit (2) | ||||||
|
Range |
Min = 250 ÷ ‘Max’ (3) | ||||||
| Default Value | ‘Max’ (3) | ||||||
| Store Supported | No | ||||||
| Description |
|
||||||
|
Notes |
(1) Available with firmware V02r20 or superior. (2) See Factor Group. (3) ‘Max’ value is calculated according to this formula: ‘Max’(User-defined velocity unit) = 3276800 * (2013.2H / 2013.1H) * (60EF.0H / 65536) Objects used in 'Max' value formula:
|