Motor_L

Index.Sub 2005.7H
Data Type Unsigned32
Access Read/Write
PDO Mappable No
Unit H x10-6

Range

Unsigned32
Default Value 2420
Store Supported Yes
Description

This object sets the motor L (inductance) used for Motor Current Regulation.

This value is used when Motor R,L detection function is disabled (bit#9 of Drive_Working_Settings_Extended object equal to 0).

The Nominal_Current of the Motor must be defined.

Notes

See Motor R, L Detection.