Motor_L_detected
Index.Sub | 2005.9H |
Data Type | Unsigned32 |
Access | Read/Write |
PDO Mappable | No |
Unit | H x10-6 |
Range |
Unsigned32 |
Default Value | -- |
Store Supported | No |
Description |
This object returns the motor L (inductance) detected with Motor R,L detection function (bit#9 of Drive_Working_Settings_Extended object equal to 1). The Nominal_Current of the motor must be defined. |
Notes |
|