Torque_window

Index.Sub
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit ‰ Nominal_Current

Range

0 to (‰ Max drive current)
Default Value 0
Store Supported Yes
Description

This object is used for Profile Torque mode (tq) and specifies a symmetrical range relative to the Target_Torque within the Target is considered having been met. If the value is set to “FFFFh” monitoring is switched off, the “Target reached” bit of Statusword is never set.

 The Target_Torque (6071.0H) value is reached if Torque_actual_value (6077.0H) is inside Torque_window (2B08.0H) for Torque_window_time (2B09.0H).

Notes

(1) Available with firmware V03r03 or superior.

  • This object is available with firmware version V02r82 or superior.