Torque_window_time

Index.Sub 2B09.0H
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit

milliseconds (ms)

Range

0 to 65535
Default Value 0
Store Supported Yes
Description

This object is used for Profile Torque mode (tq) and defines the time used to consider the Target_Torque (6071.0H) value reached.

The Target_Torque value is reached if Torque_actual_value (6077.0H) is inside Torque_window (2B08.0H) for Torque_window_time (2B09.0H).

Notes

(1) available with firmware V03r03 or superior.

  • This object is available with firmware version V02r82 or superior.