Touch_Probe_Status
| Index.Sub | 60B9.0H | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Data Type | Unsigned16 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Access | Read Only | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| PDO Mappable | TX_PDO (1) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Unit | -- | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Range |
-- | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Default Value | 0000H | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Store Supported | No | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Description |
This object provides the status of the Touch Probe.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Notes |
(1) Available with firmware V02r20 or superior.
|