HOME.IPEAKACTIVE
Description
HOME.IPEAKACTIVE allows the user to choose a different current limit during homing.
HOME.IPEAKACTIVE = 0: The current limits from the current loop are used.
HOME.IPEAKACTIVE = 1: HOME.IPEAK is used to limit the current during homing.
In Homing Modes 8, 9, 10 and 12, if HOME.IPEAKACTIVE is set to 0, the IPEAK limit will only remain until reference position is found and is deactivated before HOME.DIST is reached in homing procedure.
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-14-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | No |