IL.CMDU

Description

This parameter sets the user current command value.

The current command value, which is provided to the current loop (IL.CMD), can be limited further using a parameter setting or I2t calculation. IL.CMDU is limited also by motor peak current, IL.LIMITN and IL.LIMITP.

For IPM motors (MOTOR.TYPE = 6), IL.CMDU is decomposed into d-component and q-component current values, as both are used for closed loop current control. The d-component value is used to set IL.DCMD, and the q-component value is used to set IL.CMD.

General Information

Type

R/W Parameter

Units

Arms

Range

Minimum range value = maximum of IL.LIMITN and -MOTOR.IPEAK

Maximum range value = minimum of IL.LIMITP and MOTOR.IPEAK

Default Value

0 Arms

Data Type

Float

See Also

DRV.IPEAK, DRV.OPMODE,DRV.CMDSOURCE

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2215 DWord Yes
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
216 4 Byte Signed Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

430

No 32 bit Yes M_01-03-00-000

Related Topics

Current Loop