JOG.ACC
Description
This parameter sets the acceleration ramp for jog moves.
General Information
Type |
NV Parameter |
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR |
Range |
0.224 to 240000008.192 rpm/s |
Default Value |
10000.000 rpm/s |
Data Type |
Float |
Start Version |
M_01-19-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |