MT.FIXEDSTOPMONITORWINDOW

Description

MT. FIXEDSTOPMONITORWINDOW specifies the window in position units within which the axis should remain. If the axis reaches a position outside this window, the fixed stop has either broken off or the fixed stop has slipped or moved (a part being milled moves). Fault 176 is triggered when the position is outside the window. Configure FAULT176.ACTION to determine whether the fault returns a fault, warning, or whether the fault is ignored. After a fault or warning the axis will return to normal position loop control.

General Information

Type

R/W

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR.

Range

N/A

Default Value

0

Data Type

Float

Start Version

M_01-13-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

Related Topics

Motion Tasks

Fixed Stop

MT.FIXEDSTOPFOLLOWINGERROR

MT.FIXEDSTOPCURRENT