PL.KP

Description

PL.KP sets the proportional gain of the position regulator PID loop.

General Information

Type

NV Parameter

Units

(rev/s)/rev

Range

0 to 2,147,483.008 (rev/s)/rev

Default Value

100 rps/rev

Data Type

Float

See Also

PL.KI,

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3542h/0 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2302 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
303 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

604

No 32 bit No M_01-03-00-000

Related Topics

PL.ERR | PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop