AXIS#.MOTOR.LQLL

Description

This parameter is the motor line-to-line quadrature (torque producing) axis inductance.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mH

Range

1 to 232 mH

Default Value

4

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen AXIS1.MOTOR.LQLL 0x500B 0x14 UDINT 1000:1 - RW False
AXIS2.MOTOR.LQLL 0x510B 0x14 UDINT 1000:1 - RW False