AXIS#.VL.FBSOURCE

Description

This parameter determines the feedback source to be used by the velocity loop.

Value Definition
0 Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation
1 Selects FB1 (connector X1)
2 Selects FB2 (connector X2)
3 Selects FB3 (connector X23)
4 Selects FB4 (connector X21)
5 Selects FB5 (connector X22)

  • If Axis 2 has been configured to use gantry command source (AXIS#.CMDSOURCE = 4) and the gantry is active (GANTRY.STATE = 3), if this keyword is changed, it will set the gantry state back to "pending homing" (GANTRY.STATE = 1). See GANTRY.HOME.REQUIRED documentation for more details.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.FBSOURCE

5011h

24h

Unsigned8

-

-

Read/Write

No

AXIS2.VL.FBSOURCE

5111h

24h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.FBSOURCE

6026

178A

Unsigned8

Read/Write

-

AXIS2.VL.FBSOURCE

71562

1178

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.FBSOURCE

6026

Unsigned8

Read/Write

-

Related Topics

Velocity Loop