FB#.RES

Description

FB#.RES reports the resolution of the feedback device. The drive calculates its value based on the encoder characteristics.

FB#.RES is not necessarily the number of counts per revolution or pole pair for the position reported by FB#.P, as FB#.P always has 32 bits of single-turn or single pole-pair resolution.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: Counts/revolution

Range

N/A

Default Value

N/A

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.