AXIS#.SAFEPARAM.SDB.DELAYBEFOREDIAGNOSE

Description

Indicates the time in milliseconds from the Safe Dynamic Brake (SDB) output is triggered until the digital input is read back and compared.

Context

For complete SDB information refer to SDB (Safe Dynamic Brake).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

1 ms to 60,000 ms

Default Value

1 ms

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDB.DELAYBEFOREDIAGNOSE

3158h

03h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SDB.DELAYBEFOREDIAGNOSE

3158h

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDB.DELAYBEFOREDIAGNOSE

3258h

03h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDB.DELAYBEFOREDIAGNOSE

3258h

04h

Unsigned16

-

-

Read/Write

No