AXIS#.SAFEPARAM.SDB.DELAYBEFORESWITCHING

Description

Indicates the time in milliseconds from STO being activated until the Safe Dynamic Brake (SDB) relay is energized.

Parameters Editor Delay Before Switching (tSDB)

Context

For complete SDB information refer to SDB (Safe Dynamic Brake).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

1 ms to 60,000 ms

Default Value

1 ms

Data Type

Integer

Stored in Non-Volatile Memory

No