AXIS#.SAFEPARAM.SDB.READBACKSOURCE

Description

Indicates the digital input that is used for the read back input.

Value Description

0

Not used

1

Safe Input 1

2

Safe Input 2

3

Safe Input 3

4

Sage Input 4

5

Safe dual input 1

6

Safe dual input 2

 

Context

For complete SDB information, refer to SDB (Safe Dynamic Brake).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 or 6

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDB.READBACKSOURCE

3158h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDB.READBACKSOURCE

3258h

02h

Unsigned8

-

-

Read/Write

No