AXIS#.SAFEPARAM.STO.FUNCTIONACTIVATION

Description

Indicates how the function can be activated. For Safe Torque Off (STO), the function is ready for activation.

Value

Description

1

Ready for activation

 

Parameters Editor with the Function Activation value circled

Context

For complete STO information refer to STO (Safe Torque Off).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.54

General Information

Type

Read/Write

Units

N/A

Range

1

Default Value

Axis 1 – 1 (Ready for activation)
Axis 2 – 1 (Ready for activation)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.STO.FUNCTIONACTIVATION

3152h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.STO.FUNCTIONACTIVATION

3252h

01h

Unsigned8

-

-

Read/Write

No