SAFEPARAM.SOUTDUAL#.SOURCE
Description
When outputs are configured for dual outputs, this controls what safety function will trigger the safe output.
WorkBench will not allow the user to select this setting unless the corresponding SOUTDUAL# is enabled. See SAFEPARAM.SOUTDUALx.EN. |
Value | Description | Value | Description | Value | Description | Value | Description |
---|---|---|---|---|---|---|---|
0x00 | Off, no output signal driven | 0x13 | SLS – Axis 2 Instance 2 | 0x26 | SAR – Axis 2 Instance 1 | 0x39 | SCA – Axis 2 Instance 2 |
0x01 | STO – Axis 1 | 0x14 | SLS – Axis 2 Instance 3 | 0x27 | SAR – Axis 2 Instance 2 | 0x3A | SCA – Axis 2 Instance 3 |
0x02 | STO – Axis 2 | 0x15 |
SSM – Axis 1 |
0x28 | SAR – Axis 2 Instance 3 | 0x3B | SDB – Axis 1 |
0x03 | SS1 – Axis 1 Instance 1 | 0x16 | SSM – Axis 2 | 0x29 | SLI – Axis 1 Instance 1 | 0x3C | SDB – Axis 2 |
0x04 | SS1 – Axis 1 Instance 2 | 0x17 | SSR – Axis 1 Instance 1 | 0x2A | SLI – Axis 1 Instance 2 | 0x3D | SBC – Axis 1 |
0x05 | SS1 – Axis 1 Instance 3 | 0x18 | SSR – Axis 1 Instance 2 | 0x2B | SLI – Axis 1 Instance 3 | 0x3E | SBC – Axis 2 |
0x06 | SS1 – Axis 2 Instance 1 | 0x19 | SSR – Axis 1 Instance 3 | 0x2C | SLI – Axis 2 Instance 1 | 0x3F | SBA – Axis 1 |
0x07 | SS1 – Axis 2 Instance 2 | 0x1A | SSR – Axis 2 Instance 1 | 0x2D | SLI – Axis 2 Instance 2 | 0x40 | SBA – Axis 2 |
0x08 | SS1 – Axis 2 Instance 3 | 0x1B | SSR – Axis 2 Instance 2 | 0x2E | SLI – Axis 2 Instance 3 | 0x43 | Ready signal (always on) |
0x09 | SS2 – Axis 1 Instance 1 | 0x1C | SSR – Axis 2 Instance 3 | 0x2F | SLP – Axis 1 Instance 1 | 0x45 | Restart acknowledge request – Axis 1 |
0x0A | SS2 – Axis 1 Instance 2 | 0x1D | SDIp – Axis 1 | 0x30 | SLP – Axis 1 Instance 2 | 0x46 | Restart acknowledge request – Axis 2 |
0x0B | SS2 – Axis 2 Instance 1 | 0x1E | SDIp – Axis 2 | 0x31 | SLP – Axis 1 Instance 3 | 0xFF | Always On |
0x0C | SS2 – Axis 2 Instance 2 | 0x1F | SDIn – Axis 1 | 0x32 | SLP – Axis 2 Instance 1 | ||
0x0D | SOS – Axis 1 | 0x20 | SDIn – Axis 2 | 0x33 | SLP – Axis 2 Instance 2 | ||
0x0E | SOS – Axis 2 | 0x21 | SLA – Axis 1 | 0x34 | SLP – Axis 2 Instance 3 | ||
0x0F | SLS – Axis 1 Instance 1 | 0x22 | SLA – Axis 2 | 0x35 | SCA – Axis 1 Instance 1 | ||
0x10 | SLS – Axis 1 Instance 2 | 0x23 | SAR – Axis 1 Instance 1 | 0x36 | SCA – Axis 1 Instance 2 | ||
0x11 | SLS – Axis 1 Instance 3 | 0x24 | SAR – Axis 1 Instance 2 | 0x37 | SCA – Axis 1 Instance 3 | ||
0x12 | SLS – Axis 2 Instance 1 | 0x25 | SAR – Axis 1 Instance 3 | 0x38 | SCA – Axis 2 Instance 1 |
Context
For more information, see Safe Digital Outputs
Related safety parameters:
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-01-02-000 |
|
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0x00-0xFF |
Default Value |
0x00 (Off) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
SAFEPARAM.SOUTDUAL1.SOURCE |
3102h |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
SAFEPARAM.SOUTDUAL2.SOURCE |
3102h |
04h |
Unsigned8 |
- |
- |
Read/Write |
No |