SOUT#.STATE
Description
SOUT1 to SOUT4. Reads the state of one safe digital output according to the number identified in the command.
Context
For more information, seeSafe Digital Outputs
Related safety parameters:
- SAFEPARAM.SIN.DISTINCTPULSE
- SAFEPARAM.SINDUAL#.EN
- SAFEPARAM.SOUTDUAL#.EN
- SAFEPARAM.SOUTDUAL#.SOURCE
- SAFEPARAM.SOUT#.SOURCE
- SIN#.STATE
- SINDUAL#.STATE
- SOUTDUAL#.STATE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 or 1 |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |