SIN#.STATE
Description
SIN1 to SIN4. Reads the state of one safe digital input according to the number identified in the command.
Context
For more information, see Safe Digital Inputs and OSSD
Related safety parameters:
- SAFEPARAM.SIN.DISTINCTPULSE
- SAFEPARAM.SINDUAL#.EN
- SAFEPARAM.SOUT#.SOURCE
- SAFEPARAM.SOUTDUAL#.EN
- SAFEPARAM.SOUTDUAL#.SOURCE
- SINDUAL#.STATE
- SOUT#.STATE
- SOUTDUAL#.STATE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 or 1 |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |