SINDUAL#.STATE
Description
Reads the state of one safe dual digital input according to the number identified in the command. The safe dual input is composed of two physical safe inputs. The configuration of the safe dual input is determined by the safety parameters.
Usage
The state of the safe dual input is determined by the state of the two underlying safe inputs.
SIN1.STATE |
SIN2.STATE |
SINDUAL1.STATE |
---|---|---|
0 |
0 |
0 |
1 |
0 |
I/O failure |
0 |
1 |
I/O failure |
1 |
1 |
1 |
When dual channel mode is selected the drive supervises if the two inputs are in a different state for longer than 100 ms. If this occurs, an I/O failure fault is generated and the drive is put in safe-state.
Context
For more information, seeSafe Digital Inputs
Related safety parameters:
- SAFEPARAM.SIN.DISTINCTPULSE
- SAFEPARAM.SINDUAL#.EN
- SAFEPARAM.SOUT#.SOURCE
- SAFEPARAM.SOUTDUAL#.EN
- SAFEPARAM.SOUTDUAL#.SOURCE
- SIN#.STATE
- SOUT#.STATE
- SOUTDUAL#.STATE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 or 1 |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |