Analog Motion

This view allows you to configure the drive such that it follows a command from an analog signal. The diagram shows any current voltage being applied and the resulting scaled command, if applicable.

Element Image Description Parameter
Analog Input Source Select which analog input will be used. To select which analog input to use, click on the block or the edit symbol.To configure the behavior of the analog input itself, click the link labeled "Goto Analog Input [#]"

The keyword used depends on the operation mode.

Analog Actual Value   Actual voltage measured on the selected analog input.  
Analog Input Scaling Enter a factor by which to scale the analog input. The unit depends on the operation mode and user units defined for this axis.

The keyword used depends on the operation mode.

Command Actual Value   Actual value of the command. The unit depends on the operation mode and user units defined for this axis.  

Current/ Position/ Velocity/ Command

 

Clicking this item brings you to the corresponding loop view depending on the operation mode.